Product FAQs

Ask a Question

How to install Unity Pro v8.0 on a Windows 8 PC.

Title
How to install Unity Pro v8.0 on a Windows 8 PC.

Issue
Unity Pro v8.0 will not install on Windows 8.

Product Line
Unity Pro

Envirnment

Cause

Resolution

Before installing Unity Pro v8.0 you must run the UPWIN8.exe file in the Windows 8 folder on the Unity Pro v8.0 installation DVD. 

If Unity Pro v8.0 has already been installed, you must uninstall Unity Pro v8.0 and then run UPCleaner v8.0 and follow these instructions:
1. Unzip and install UPCleaner v8.0
2. Remove Unity Pro
3. Run the UPCleaner Utility
4. Run the UPWIN8.exe file in the Windows 8 folder on the Unity Pro v8.0 DVD
5. Re-install Unity Pro v8.0.
Was this helpful?
What can we do to improve the information ?