Product FAQs

Ask a Question

Is it possible to check for unused variables in SoMachine?

Title
Unused variables in SoMachine
 
Issue
A customer is trying to find his unused variables in SoMachine
 
Product Line
M258, M238, LMC058, XBTGC, HMISCU
 
Environment
SoMachine 1.0, SoMachine 2.0, SoMachine 3.0, SoMachine 3.1, SoMachine 4.1, SoMachine 4.2, SoMachine 4.3
 
Cause
N/A
 
Resolution
It is not possible to check for unused variables in SoMachine 1.0, SoMachine 2.0, SoMachine 3.0 or SoMachine 3.1, SoMachine 4.1, SoMachine 4.2, SoMachine 4.3
Was this helpful?
What can we do to improve the information ?