Product FAQs

Ask a Question

Is Open SSL used on the ADVC2 controllers?

Issue
This question stems from the newly announced Heart Bleed bug which utilizes vulnerabilities in the Open SSL protocol.

Product Line
ADVC2
ADVC

Resolution
No, Open SSL is not used on the ADVC2 controllers.

Was this helpful?
What can we do to improve the information ?