Product FAQs

Ask a Question

Which Driver do I need to select to link my Vijeo Designer V6.2 variables to the RSLogic 5000 l5k file?

The driver to select is Allen-Bradley Ethernet/IP.

Then right-click on variables and link to the L5k file.

.
Was this helpful?
What can we do to improve the information ?