Product FAQs

Ask a Question

Is SoMachine v3.1 compatible with Windows Server 2012?

No, it is not.  Somachine v3.1 is only supported on Windows XP Pro, Windows 7 Pro 32bit, and Windows 7 Pro 64bit.
Was this helpful?
What can we do to improve the information ?