Product FAQs

Ask a Question

Why are my function block not running in SoMachine basic

There is no POU assigned to the Master Task.
One POU must always exists and must be linked to the master task of the program. This POU is then called automatically whenever the program starts.
Was this helpful?
What can we do to improve the information ?