Product FAQs

Ask a Question

Can a password protected project be loaded onto an M221 via the SD card?

A password protected project can be loaded onto a M221 controller via the SD card ONLY IF there is NOT already a protected project loaded. If there is a protected project loaded to the M221, it will not load any project from the SD card. The project has to be loaded via the SoMachine Basic software.
Was this helpful?
What can we do to improve the information ?