Product FAQs

Ask a Question

How to Setup Remote connection in SoMachine v4.1?

Go into the Devices Tree and click on MyController. Hover over to the right and click on controller selection, at the bottom under connection mode picklist, select IP Address via NAT (Remote TCP).
Was this helpful?
What can we do to improve the information ?