Product FAQs

Ask a Question

Why SoMachine application need to do Create boot application operation after online change every time?

SoMachine PLC application is stored in Flash. When PLC is powered on, the applcation will be copied from Flash to RAM, and run in RAM. If you do online change, the change is just stored in RAM. So you need to do Create boot application operation to store the change in Flash. Otherwise, the change will lost when you power off PLC.

You can change the application setting with: Create implicit boot applyication on Online change. Please see attached picture
Was this helpful?
What can we do to improve the information ?