Product FAQs

Ask a Question

What is the available output amperage on a TM3AQ4 module configured for a 0-10V signal?

When the output is configured for a 0-10V analog output signal the maximum current we can deliver to the load is 10 mAmp for each of the 4 channels of the TM3AQ4 module. 10 mAmp is a Maximum value, so to not have a higher value , the Load needs to have a Resistor not below 1k Ohms.
Was this helpful?
What can we do to improve the information ?