Product FAQs

Ask a Question

How do you change the node name of a M238 with a TM2USBABDEV1 Loader Device Accessory?

Follow the instructions from the TM2USBABDEV1 Loader Device Accessory manual to generate the Application.app and Application.crc and copy them onto an USB Memory Key. The two files are created offline by going to Online / Create Boot Application. To change the node name you will have to add an additional file, LateConf.bin. This file can be copied from the M238 while connected with SoMachine by going to MyController / FIles / Runtime. The file can be opened and the node name modified in Notepad. The file can also be created with Notepad with only one line containing the node name (ex: MyMachine) and then the file name can be changed to LateConf.bin
 
Was this helpful?
What can we do to improve the information ?