Product FAQs

Ask a Question

Why can't I program the Pulse Width MOdulation Function Block in SoMachine Basic ver 1.3?

If the function block is bank when inserted into a rung, the Pulse Generators have not been setup in your Configuration. In the Configuration Tab under "My Controller" select "Pulse Generators" Select %PWM0 configuration and set the Time base and Preset for the pulse generator. Select apply and now you can use the function block in your logic.
Was this helpful?
What can we do to improve the information ?