Product FAQs

Ask a Question

What is the correspondence between the SoMachine variable i_wClockBatterystatus read level and BAT LED?

When i_wClockBatterystatus value is less then 25 and higher then zero it corresponds to BAT LED flashing red, indicating that the battery charge is low.
When i_wClockBatterystatus value is equal to 0  it corresponds to BAT LED solid red ON , indicating that the battery needs to be replaced.
Was this helpful?
What can we do to improve the information ?