Product FAQs

Ask a Question

What is the default IP address on the M251 controllers?

The default IP addresses are:
  • 11.11.x.x. for Ethernet 1
  • 10.10.x.x. for Ethernet 2 (only available on TM251MESE)
NOTE: The 2 IP addresses must not be in the same IP network.
The last 2 fields in the default IP address are composed of the decimal equivalent of the last 2 hexadecimal bytes of the MAC address of the port.
The MAC address of the port can be retrieved on the label placed on the front side of the controller.
The default subnet mask is Default Class A Subnet Mask of 255.0.0.0.

NOTE: A MAC address is always written in hexadecimal format and an IP address in decimal format. Convert the MAC address to decimal format.
Example: If the MAC address is 00.80.F4.01.80.F2, the default IP address is 10.10.128.242.

NOTE: To take into account the new IP address after the download of a project, reboot the controller by doing a power cycle.
Was this helpful?
What can we do to improve the information ?