Product FAQs

Ask a Question

Is there a conversion tool available to convert a TSX37 Micro project to a Somachine controller?

Issue:
Is there a conversion tool available to convert a TSX37 Micro project to a Somachine controller?

Product Line:
TSX 37 Micro, PL7, Somachine

Environment:


Cause:


Resolution:
No, there is not a conversion tool that will convert a TSX37 Micro to a Somachine controller.  The only conversion we have is to go from TSX37 Micro to Unity Pro using the exported *.FEF file.
Was this helpful?
What can we do to improve the information ?