Product FAQs

Ask a Question

What is the maximum number of Modbus RTU connections that an XBTGT can support?

The maximum number of Modbus RTU connections that an XBTGT can support is 32. 
Was this helpful?
What can we do to improve the information ?