Product FAQs

Ask a Question

What is the 2nd motor parameters in ATS48?


The 2nd set of parameters are used when we have two different motors are to be operated separately where we can save the parameters of each motor separately & switch between the two configurations using a logic input ( the logic input in the I/O menu is to be set to LIS, so for example LI3 or LI4= LIS ) so they can be started one after the other using a single soft starter
Noting that switching from one parameter set to another can be done if ATS is not driving the motor (ATS in stop state). Below attached those parameters
Was this helpful?
What can we do to improve the information ?