Product FAQs

Ask a Question

Can the application on a broken XBTGT be transferred to a new replacement?

If the XBTGT does not have the VDZ file backed up on it, on either the Secondary or Optional drive, then it is not possible to transfer the existing application on the XBTGT to a new replacement. If the VDZ is available, then the user may use the VDZ file to download to the new replacement using Vijeo Designer.
Was this helpful?
What can we do to improve the information ?