Product FAQs

Ask a Question

Can you use Multiple Download to download an application to an HMI or HMI controller that has an older Vijeo Designer Runtime with Vijeo Designer 6.2 ?

Multiple Download used to download an application to an HMI or HMI controller that has an older Vijeo Designer Runtime on it will not automatically update the Runtime. The user must manually upgrade Vijeo Designer Runtime by using Vijeo Designer Runtime Installer. This tool can be launched from the "Maintenace" button of SoMachine Central -> select "Download Firmware HMI" to launch.
Was this helpful?
What can we do to improve the information ?