Product FAQs

Ask a Question

How can I update SoMachine to version 4.1 SP1.2

Steps to install SoMachine V4.1 SP1.2.
 
1-Install SoMachine V4.1 SP1.  The link is a complete install. 
 
2- Use the Schneider Electric Software Update (SESU) to update SoMachine to version 4.1 SP1.2
 
3- Use SESU to update Vijeo Designer V6.2 with SP3.1
 
Note:
Vijeo Designer V6.2 SP3.1 is compatible with SoMachine V4.1 SP1.1 and SP1.2
Vijeo Designer V6.2 SP3 cannot be installed on top of SoMachine V4.1 SP1 and previous version.
 
Was this helpful?
What can we do to improve the information ?