Product FAQs

Ask a Question

Is it possible to download to a Magelis HMISCU with SoMachine using the IP address connection mode?

SoMachine V4.1 SP1.2 does not support this feature.  It is only possible to download using the Node name connection mode.


This download method below is not supported with the HMISCU.
Was this helpful?
What can we do to improve the information ?