Product FAQs

Ask a Question

What are the certification of compliance for the 3090 split core CTs?

Issue
What are the certification of compliance for the 3090 split core CTs?

Product Line
3090 SCCT0xx and 3090 SCCT1x4

Environment
Certification documentation

Cause
Customer needs documentation that the 3090 split core CT's are certified to an applicable standard.

Resolution
The American standard is UL 61010-1B, and the Canadian standard is CAN/CSA-C22.2 No. 61010-1-2004.
The design of these CT's has been evaluated and tested to these standards, and been found to meet them.

Was this helpful?
What can we do to improve the information ?