Product FAQs

Ask a Question

Whycan't I to load the application to a M238 using the TM2USBADEV1 loader after upgrading to SoMachine V4.1?

The TM2USBADEV1 is not possible to load a application into the M218/M238 controller when no application is present.
This error was reproduced with firmware versions M218v4.0.1.24.mfw and TM238LFDC24DT_V4.0.1.21.mfw on SoMachine-4.1.0.0-RC1_14.02.19.02.

Firmware version 0009_00 resolves this issue.



 
Was this helpful?
What can we do to improve the information ?