Product FAQs

Ask a Question

What are the System Requirements for SoMachine Basic v1.3 SP2?

The minimum system requirements for the PC on which SoMachine Basic software is installed are:
  • Intel Core 2 Duo processor or greater
  • 1 GB RAM
  • The 32- or 64-bit version of one of the following operating systems:
    • Microsoft Windows XP Service Pack 3
    • Microsoft Windows 7
    • Microsoft Windows 8
Was this helpful?
What can we do to improve the information ?