Product FAQs

Ask a Question

Can I use an Excel spreadsheet as an OPC client to communicate to the Somachine OPC server?

Issue:
Can I use an Excel spreadsheet as an OPC client to communicate to the Somachine OPC server?

Product Line:
Somachine OPC, Codesys OPC

Resolution:
Yes, Excel can be used as OPC Client.

It requires Graybox OPC DA Automation Wrapper and a VBA program to access the OPC data through Excel.

Attached is a sample.
Was this helpful?
What can we do to improve the information ?