Product FAQs

Ask a Question

What is the number of Ethernet/IP adapter assembly sizes for TM258 / LMC058 and TM241 / TM251 controllers?

Starting with SoMachine 4.1 SP2, Ethernet/IP adapter assembly sizes are extended to 120 words for TM258 / LMC058 and TM241 / TM251 controllers
This information is also true for SoMachine 4.2
Was this helpful?
What can we do to improve the information ?