Product FAQs

Ask a Question

Can I connect to the M221 controller remotely?

The M221 with firmware v1.3.3.3 usnig SoMachine basic v1.3SP2 can be accessed remotely.

You must use the remote lookup field to enter the public IP address of the router.

The M221 uses internal port 502.

For more information on how to configure port forwarding please see the link below: 
http://www.wikihow.com/Set-Up-Port-Forwarding-on-a-Router 
Was this helpful?
What can we do to improve the information ?