Product FAQs

Ask a Question

What is the number of Ethernet/IP adapter assembly sizes for TM258 / LMC058 and TM241 / TM251 controllers?

Starting with SoMachine 4.1 SP2, a new firmware version: 4.0.2.xx will be delivered. In this new version, the maximum size of words increased for Ethernet IP Adaptor : %IW 120 words - %QW 120 words (it was: 40 )
Was this helpful?
What can we do to improve the information ?