Product FAQs

Ask a Question

How Can I Enable and Configure Analog Inputs on CANopen OTB in SoMachine?

To  enable and Configure Analog Inputs on CANopen OTB in SoMachine please follow the steps below:

1. Double-click the node of your analog CANopen device in the Devices tree.
2. In the CANopen Remote Device tab of the editor, enable the option Enable Expert Settings.
Result: Additional tabs are displayed and the Service Data Object tab is populated with information.
3. Open the Service Data Object tab and click the New... button.
Result: The Select item from object directory dialog box is displayed.
4. From the list of objects, select object 6423, enter 1 as Value, and click OK.
Result: Analog input transmission on the CANopen bus is activated. You can now configure parameters of the analog values as described in the hardware manual of your device.
Was this helpful?
What can we do to improve the information ?