Product FAQs

Ask a Question

How to establish communication between an M221 and HMIS5T using Modbus RTU?

Issue:
How to link SoMachine Basic to Vijeo Designer

Product Line:
All M221 line, all serial numbers, all localizations and languages, all revisions

Environment:
SoMachine Basic

Cause:
No I/O scanning available in M221 so workaround necessary

Resolution:
Start by creating your M221 application in SoMachine Basic, with all the needed variables, then import the .smbp file into Vijeo Designer.
Was this helpful?
What can we do to improve the information ?