Product FAQs

Ask a Question

What are the P/Ns of the key, handle, lock that comes with the standard Spacial SM/SF enclosure?

The lock accessories that comes in standard with the SF/SM enclosures are: 

1. Handle P/N NSYSFHS1 (refer to handle.jpg) 
2. Lock P/N NSYINDB51 (refer to lock.jpg) 
3. The key that comes with standard SF/SM enclosures is not referenced, but there is a metal key DB5 referenced (NSYLDB5) 
- Standard key delivered with standard SF/SM enclosures (refer to standard key.jpg) 
- Metal Key DB5 P/N NSYLDB5 (refer to NSYLDB5.jpg) 
Was this helpful?
What can we do to improve the information ?