Product FAQs

Ask a Question

What are causes for an OCF Overcurrent fault on an ATS48 soft starter?

Issue:
What are causes for an OCF Overcurrent fault on an ATS48 soft starter?

Product Line:
Altistart 48 ATS48

Environment:
All models

Cause:
Unit trips OCF

Resolution:
The ATS48 monitors the current on each phase and is detecting a much higher current than expected.  See below troubleshooting guidelines.

Was this helpful?
What can we do to improve the information ?