Product FAQs

Ask a Question

Which connection mode in Somachine to use when connecting to the HMISCU remotely through a router?

Issue:
Which connection mode in Somachine to use when connecting to the HMISCU remotely through a router?

Product Line:
Remote TCP, IP Address via NAT (Remote TCP), Nodename via NAT (Remote TCP)

Environment:


Cause:


Resolution:
Use the ‘Nodename via NAT (Remote TCP)’ connection mode to connect to the HMISCU remotely.  

To utilized this feature in the HMISCU, please update to SoMachine to V4.1 SP2 or higher.

 
Was this helpful?
What can we do to improve the information ?