Product FAQs

Ask a Question

PME 8.1 Dashboards stay at Loading... and do not populate

Issue
User opened dashboards, the application loads however the list of dashboards does not get past "Loading..."

Product
Power Monitoring Expert 8.1

Environment
Internet Explorer running on Windows Server OS

Cause
An update to Windows disabled Active Scripting by default

Resolution
2 possible resolutions

1) Use Firefox browser, (or Chrome if only interested in application that do not use silverlight)

2) Change the setting in Internet Explorer to enable Active Scripting.
*Warning: Only complete this work if the server is protected behind a firewall or on a private network. Enabling Active Scripting can expose the server to security risks

a) Open Internet Explorer
b) Under Tools -> Internet options -> Security, Select the zone the PME server is located in. 
Note: if Active Scripting is disabled in the Internet zone, the setting will need to be enabled.
c) Under Security Setting for this zone, select the custom button
d) Scroll Down to the Scripting section, ensure that Active Scripting is enabled.


e) Server may need to be rebooted for the changes to take effect
Was this helpful?
What can we do to improve the information ?