Product FAQs

Ask a Question

Looking to buy the patch cable VDIP184546050

Issue:
I can't find cable VDIP184546050 under MySchneider

Product Line:
M221 controllers

Resolution:
The VDIC cables are not UL marked so they cannot be sold in North America.
Some existing 490NT**** cables that are already UL marked can do the job and meet the specs.

Some of the documents related to the product only have the VDIC numbers. Others contain both.

This catalog has both. 
http://download.schneider-electric.com/files?p_Reference=DIA3ED2140109EN&p_EnDocType=Catalog&p_File_Id=2192337703&p_File_Name=DIA3ED2140109EN+%28web%29.pdf
The 490NTW00005U is the same length as the VDIP184546050.
Was this helpful?
What can we do to improve the information ?