Product FAQs

Ask a Question

I would like to get the characteristics of resistance to voltage dips for LTMCU


As we know that LTMCU has following functions

The LTMCU can be used to:
> configure parameters for the LTMR controller,
> display information about the LTMR controller configuration and operation,
> monitor detected faults and warnings detected by the controller,
> control the motor locally using the local control interface.


The LTMCU receives the supply voltage via the LTMR controller , so the resistance to voltage dips of LTMCU will be same as that of LTMR controller. Please refer the attached file.


If the supply voltage dip goes down to 0V for a time not greater than 3ms we guarantee that TeSys T will support it.
If the supply voltage dip goes down to 70% of nominal voltage ( 16.8VDC for 24VDC product and 70VAC for 100 to 240 ) for a time not greater than 500ms we guarantee that TeSys T wil support it.
Was this helpful?
What can we do to improve the information ?