Product FAQs

Ask a Question

Can we add additional auxiliaries to capacitor bank contractors LC1DTK**, LC1DWK12**?

We have in–built instantaneous auxiliary contact blocks available in our capacity duty contactors. There is no separate accessory available for the Capacitor switching contactor.
You can add a side mounting contact block type LAD8N**. This will provide you with 2 Additional Auxiliary contacts.
However, if you wish to increase the auxiliary contacts further, then use an Auxiliary contactor type CAD32 /CAD50 in conjunction with the Main Contactor.

 
 

Was this helpful?
What can we do to improve the information ?