Product FAQs

Ask a Question

Used Convert Device in Somachine to change the Magelis target type but Vijeo Designer does not reflect the change. How to resolve this issue?

Issue:
Used Convert Device in Somachine to change the Magelis target type but Vijeo Designer does not reflect the change.  How to resolve this issue?

Product Line:
Magelis, Convert Device, Somachine, Change Magelis

Environment:


Cause:


Resolution:
To resolve the issue, use Convert Device and convert it back to the original Magelis target.  Then use Convert Device again to convert to the new Magelis target.  Once that is complete goto Vijeo Designer confirm if the new target shows up.
Was this helpful?
What can we do to improve the information ?