Product FAQs

Ask a Question

Read actual torque on a LXM32 in SoMachine

Issue:
Read LXM32 actual torque in SoMachine

Product Line:
LXM32M, LXM32A, LXM32C

Resolution:
The easiest way to read the actual torque on a LXM32 drive is to use the function block MC_ReadActualTorque_LXM (See attached screenshot)
Was this helpful?
What can we do to improve the information ?