Product FAQs

Ask a Question

Fuse rating for LMC058 motion controller

Issue:
What fuses to use to protect the LMC058 motion controller?

Product Line:
LMC058

Resolution:
The time delay Type T fuses that should be used with our PLC range are similar to this: 
https://www.homehardware.ca/en/rec/index.htm/Plumbing-Electrical/Electrical/Fuses/Household/Miscellaneous/2-Pack-1-Amp-250-Volt-Time-Delay-Glass-Fuses/_/N-ntjyh/R-I3644526 
There are ones for 1 Amp and 3 Amps. See attached
Was this helpful?
What can we do to improve the information ?