Product FAQs

Ask a Question

Replacement of Berger Lahr servo motor SER31117/4L3S

Issue:
Replacement of Berger Lahr servo motor model SER31117/4L3S

Product Line:
Lexium SER

Resolution:
We do not offer any motors with the same exact frame size so we can only match the speed and torque specs of the motor. 
The new motor will be a BMH1003P01F2A, which has a higher torque (8.2 N.m instead of 6.6 N.m and a slightly higher rotor inertia (9.405 Kg cm2 instead of 8 Kg cm2) 
If LXM05 servo drive is used, you can keep it as it is compatible with the new BMH motor. 
Was this helpful?
What can we do to improve the information ?