Product FAQs

Ask a Question

Replacement of servo drive LXM05AD42M3X

Issue:
I need to replace the LXM05AD42M3X drive

Product Line:
LXM05

Resolution:
To replace the LXM05AD42M3X you need: 
- Servo drive: LXM32MD30N4 
- Power cable: VW3M5101R30 (30 = 3m, 50 = 5m...) 
- Encodeur cable: VW3M8102R30 
- CANOpen card: VW3A3608 (if the control is done via CANOpen) 
- Termination RJ45 resistor: TCSCAR013M120 (for CANOpen control) 

You might have to update the motor firmware if the date of manufacture DOM is older than 15.07.2009 (verify motor name plate to get DOM). 
Was this helpful?
What can we do to improve the information ?