{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What are the power consumption values for closing, holding & tripping for CTV1 vacuum contactor (mechanical latching version)?

Control circuit burden/current for CTV1 contactor can be given as follows:

A) For Magnetically held version:
Closing: 670VA (AC) - 700W (DC)
Holding: 85VA (AC) - 85W (DC)
Tripping: Not applicable (magnetically held contactor)

B) For Mechanically held (Latched) version:
Closing: 670VA (AC) - 700W (DC)
Holding: 85VA (AC) - 85W (DC)
Tripping: 4.8A (DC) Max​

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.