Product FAQs

Ask a Question

Velocity scaling on LXM28 drive

Issue:
How to scale the velocity on a LXM28 drive?

Product Line:
LXM28

Resolution:
On the Lexium 28, there is no separate velocity or ramp scaling. There is only a position scaling.
Therefore the speed scaling depends on the setting of the position scaling.
With CANopen control, the position scaling will be calculated by 6092:1 = Feed (default setting: 1280000) and 6092:2 = Shaft revolutions (default setting: 1).
The UNIT for the speed input value is: pulses (Increments) per second, which means for the default scaling factor (1280000/1):  With a speed input value of 1280000, the motor moves with a speed of 1 rps = 60 rpm.
If you want to have a scaling in rpm you have to set the scaling factor: 6092:1 Feed = 60 and 6092:2 Shaft revolutions = 1
With this setting, you´ll have a speed scaling in RPM, and the motor turns with a speed of 60 RPM when you enter a speed input value of 60.
You can also enter the values for the scaling factor into the SDO list in SoMachine.
Was this helpful?
What can we do to improve the information ?