Product FAQs

Ask a Question

Fuse and circuit breaker rating for LXM32

Issue:
What is the fuse or circuit breaker rating for LXM32 drives?

Product Line:
LXM32

Resolution:
For 115VAC and 230VAC drives, the maximum fuse to be connected upstream is 25 Amps, Class CC or J as per UL 248-4, alternatively circuit breakers with B or C characteristic.
For 400VAC and 480VAC drives, the maximum fuse to be connected upstream is 30/32 Amps, Class CC or J as per UL 248-4, alternatively circuit breakers with B or C characteristic.
Was this helpful?
What can we do to improve the information ?