Product FAQs

Ask a Question

Getting error E4102 on LXM32 drive

Issue:
Getting E4102 on LXM32 drive

Product Line:
LXM32

Resolution:

E4102 means "power stage I2t".The drive creates a warning message (WarnLatched bit 30) and reduces to nominal current. There's no stop reaction in case of warnings.
A warning is an error class 0 meaning there's no reaction in transition. If there are warnings (error class 0), the two dots to the right of the 7-segment display (2) flash.
The parameters _WarnLatched and _SigLatched contain information on warnings and errors.
It's also possible to define an output for a warning or error.
The reason why the speed could drop to 0 is maybe because of reduced current or if there has been a stop command from the PLC.

Was this helpful?
What can we do to improve the information ?