Product FAQs

Ask a Question

Looking for the pinout for encoder cable VW3M8101R30

Issue:
Pinout for encoder cable VW3M8101R30 that goes between the BSH servo motor and the LXM05 servo drive

Product Line:
LXM05

Resolution:
The pinout is attached, as well as an extract from the LXM05 manual showing the different part numbers of the cable.
Was this helpful?
What can we do to improve the information ?