Product FAQs

Ask a Question

Setting up MBP_MS-TR block in Quantum PLC to read 3X Registers over TC-PIP from remote device.

Here is attached technical note and mbp_mstr manual.  Incase if its required to setup for coil read it must be setup for Function 15 generic Modbus request and 01 for coil read.
Was this helpful?
What can we do to improve the information ?