Product FAQs

Ask a Question

Which parameters have been changed in a LXM32 SoMove file?

Issue:
How to know which parameters have been changed in a LXM32 SoMove file

Product Line:
SoMove, LXM32

Resolution:
1- First, make a SoMove file with default values (FSU) and then compare with the SoMove file that has the edited parameters.
2- Both configuration files will be displayed on the screen and the highlighted values are those parameters that are different (See attached)
Was this helpful?
What can we do to improve the information ?