Product FAQs

Ask a Question

Does the LXM32S work with a Bosch Rexroth PLC?

Issue:
Does the Sercos III LXM32S work with a Bosch Rexroth PLC?

Product Line:
LXM32S

Resolution:
Currently, it is not possible to use LXM32S as a 3rd party drive with SERCOS III in a Bosch Rexroth system. 
The LXM32S only works in combination with the LMC078 because of a special implementation of SERCOS III. 
Was this helpful?
What can we do to improve the information ?